Technical FAQs

Ask a Question

What is the replacement for KAL362251595?

Issue:
What is the replacement for KAL362251595?

Product Line:
Legacy Molded Case Circuit Breaker KAL series

Environment:
The KAL Series is obsolete. It can be replaced with the PowerPact J frame. Any operating mechanisms would also have to be replaced and if the K frame was in a MCC bucket then the entire bucket will have to be replaced.

Cause:
A replacement is needed for the KAL362251595 since it is obsolete.

Resolution:
1595 is a combination of 2a2b auxiliary switches and 120Vac under voltage trip (UVR).
The replacement for the KAL breaker  would be a JDL36225 or JGL36225 (depending on the AIC rating desired) and (2) S29450 Auxiliary switches and (1) S29406 120Vac UVR coil or order JDL/JGL36225ABUA to have the auxiliary switches and UVR factory installed.

The KAL Series is obsolete. It can be replaced with the PowerPact J frame. Any operating mechanisms would also have to be replaced and if the K frame was in a MCC bucket then the entire bucket will have to be replaced.


CTA-ID : 2789
Was this helpful?
What can we do to improve the information ?