Technical FAQs

Ask a Question

What is the consumption of the latch control coil for 8903LX lighting contactor?

Based on quantity of poles provided as listed below:

2 - 4 pole devices at 60 hertz = Inrush 150 vA.
2 - 4 pole devices at 50 hertz = Inrush 140 vA.

8 - 12 pole devices at 60 hertz = Inrush 180 vA.
8 - 12 pole devices at 50 hertz = Inrush 170 vA.

Note: there is no sealed current consumption on mechanically held devices.


CTA-ID : 4858
Was this helpful?
What can we do to improve the information ?