Technical FAQs

Ask a Question

Customer has an XF9D251 but wants to replace it with a 3 pole. Can`t find any info on it.

It is an overtravel limit switch that uses a D Line contactor. It is a 3 or 4 pole device as it stands. Information is available in the Cite.

CTA-ID : 4888
Was this helpful?
What can we do to improve the information ?