Technical FAQs

Ask a Question

What is the 208 volt replacement coil for an 8502A Contactor?

31012-400-49 for 60hz, 50hz is not available. This 208 vac replacement coil is for Series B & C only, Series A coils are obsolete and no longer available. This also applied to all 8536A, 8538A, 8539A, 8606A, 8630A, 8640A, 8702A, 8736A, 8738A, 8739A, and 8810A, devices. For enclosed devices, the series information is based on device and not enclosure nameplate.

CTA-ID : 4708
Was this helpful?
What can we do to improve the information ?