Technical FAQs

Ask a Question

Are replacement enclosures available for 2510 FG1 starters?

Issue: Are replacement enclosures available for 2510 FG1 starters?

Product Line: 2510 type F manual starters

Environment: Products sold and used in the United States

Cause: Need a part number for the replacement enclosure for the 2510 type FG1 starter

Resolution: The 9991 EN1 is the replacement enclosure only. It includes the frame and cover. The frame is the metal back portion of the surface mounted enclosure. The cover is the non-metallic front portion of the enclosure.

Please note that the switch or starter; nameplate; handle guard and clear lens (if used) are NOT included with the 9991 EN1.

This also applies to 2510 FG1P, 2510 FG2, 2510 FG2P, 2510 FG3, 2510 FG3P, 2510 FG4, 2510 FG4P, 2510 FG5, 2510 FG5P, 2510 FG6, 2510 FG6P, 2510 KG1, 2510 KG1A, 2510 KG1AG, 2510 KG1B, 2510 KG 1BG, 2510 KG2, 2510 KG2B, 2510 KG2BG, 2510 KG2C, 2510 KG2CG, 2510 KG3, 2510 KG3A, 2510 KG3AG, 2510 KG3B, 2510 KG3BG, 2510 KG4, 2510 KG4B, 2510 KG4BG, 2510 KG4C, 2510 KG4CG, 2510 KG5, 2510 KG5A, 2510 KG5AG, 2510 KG5B, and 2510 KG5BG devices.


CTA-ID : 4497
Was this helpful?
What can we do to improve the information ?