Technical FAQs

Ask a Question

What is the consumption of the control coil for 8502SE contactor?

For 2 & 3 pole devices 700 VA inrush and 46 VA sealed for 60 hertz or 678 VA inrush and 47 VA sealed for 50 hertz. For & 5 pole devices 1185 VA inrush and 85 VA sealed for 60 hertz or 1260 VA inrush and 89 VA sealed for 50 hertz. This also applies to all 8536SE, 8538SE, 8539SE, 8606SE, 8630SE, 8640SE, 8702SE, 8736SE, 8738SE, 8739SE, 8810SE, 8903SQ, 8910DPA122, 8910DPA123, 8910SYD138, 8940 Size 3 except ``NP``, 8941NE, and 8941CE devices.


CTA-ID : 4790
Was this helpful?
What can we do to improve the information ?