Technical FAQs

Ask a Question

What is the 110-115 volt replacement coil for a Type SA NEMA Size 00 contactor or starter?

The 110-115 vac replacement coil for all Size 00 (i.e., SA) contactors depends on the device`s series or revision. The following outlines the part by Series number: Series A 50hz - 31041-400-42, Series B - 9998SAC45. For enclosed devices, the series information is based on device and not enclosure nameplate.

CTA-ID : 4798
Was this helpful?
What can we do to improve the information ?