Technical FAQs

Ask a Question

What is the replacement 120 volt coil for a Type SG NEMA Size 5 contactor or starter?

The 120 VAC replacement coil for all Size 5 contactors and starters depends on the device`s series or revision. The following outlines the part by Series number: Series A 60hz - 31096-400-09, 50hz 31096-400-10, Series B - 50/60hz - 31096-320-50. For enclosed devices, the series information is based on device and not enclosure nameplate.


CTA-ID : 4800
Was this helpful?
What can we do to improve the information ?