Technical FAQs

Ask a Question

What is the 208 volt replacement coil for a Type SA NEMA size 00 contactor or starter?

The 208 vac replacement coil for all Size 00 contactors depends on the device`s series or revision. The following outlines the part by Series number: Series A 60 hz- 31041-400-48, Series B - 60 hz- 9998SAC52. For enclosed devices, the series information is based on device and not enclosure nameplate.


CTA-ID : 4801
Was this helpful?
What can we do to improve the information ?