Technical FAQs

Ask a Question

What is the replacement 240 volt coil for a Type SG NEMA Size 5 contactor or starter?

The 240 VAC replacement coil for all Size 5 contactors and starters depends on the device`s series or revision. The following outlines the part by Series number: Series A 60hz - 31096-400-18, Series B - 50/60hz - 31096-320-52. For enclosed devices, the series information is based on device and not enclosure nameplate.

CTA-ID : 4807
Was this helpful?
What can we do to improve the information ?