Technical FAQs

Ask a Question

What is the replacement 550 volt coil for a Type SG NEMA Size 5 contactor or starter?

The 550 VAC replacement coil for all Size 5 contactors and starters depends on the device`s series or revision. The following outlines the part by Series number: Series A 50hz - 31096-400-29. There is no Series B coil for this application. For enclosed devices, the series information is based on device and not enclosure nameplate.


CTA-ID : 4817
Was this helpful?
What can we do to improve the information ?