Technical FAQs

Ask a Question

What is the replacement for the IF, IFL, FI, FIL breaker?

Issue:
What is the replacement for the IF, IFL, FI, FIL breaker?

Product Line:
IF, IFL, FI, FIL current limiting breakers

Environment:
This includes all of the obsoleted IF, IFL, FI and FIL breakers.

Cause:
Need to know what replaced the current limiting breakers that are now obsolete.

Resolution:
They have all been replaced by the PowerPact HR frame electronic trip breaker. The "R" interrupt breaker has the following ratings: 200/200/100kA.  It is available in both unit mount (HRL) or I-Line (HRA).
Three frames are available: HR( )36060U(  )X, HR( )36100U(  )X and HR( )36150U(  )X.
Note Unit mount breakers can be 100% rated by adding a "C" before the "U". The I-Line version can only be 80% rated.

 
Was this helpful?
What can we do to improve the information ?