Technical FAQs

Ask a Question

What are the repair parts for a KA225AWK circuit breaker enclosure?

Issue:
Repair parts

Product Line:
Circuit Breaker Enclosure

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The only field replaceable parts for this enclosure are the Red/Black handle knobs located on the external operating handle. Part number 4028343850 includes the red knob, black knob and hardware for repair of one handle.


CTA-ID : 6036
Was this helpful?
What can we do to improve the information ?