Technical FAQs

Ask a Question

What are the repair parts for a LA400AWK circuit breaker enclosure?

The only field replaceable parts for this enclosure are the Red/Black handle knobs located on the external operating handle. Part number 4028343950 includes the red knob, black knob and hardware for repair of one handle.

This is obsolete without replacement.


CTA-ID : 6040
Was this helpful?
What can we do to improve the information ?