Technical FAQs

Ask a Question

Which shunt trip is required to work with the GFM modules?

Issue:
Which shunt trip is required to work with the GFM modules?

Product Line:
GFM modules for Legacy and Powerpact breakers

Environment:
Electrical distribution

Cause:
Shunt trips are required to complete the GFP system

Resolution:
For GFM150HD and GFM250JD modules, a 12 Vdc shunt trip module (Catalog No. S29382) is required in the circuit breaker.
This may be field installed or factory installed when the circuit breaker is ordered with an -SN suffix.

For the obsolete GFM100FA, GFM100KI, and GFM250KA modules, the shunt trip must be factory installed in the companion circuit breaker, suffix -G.
Was this helpful?
What can we do to improve the information ?