Technical FAQs

Ask a Question

QOU circuit breaker mounting feet part numbers

Issue:
Part numbers for QOU mounting feet

Product Line:
Circuit Breakers

Environment:
Applies to QOU circuit breakers only

Cause:
Replacements are needed for QOU mounting feet

Resolution:
For QOU mounting feet, use the following. 1 piece per kit.
1 pole - QOUMF1
2 pole - QOUMF2
3 pole - QOUMF3

For bulk packs:
QOUMF1B - 80 pieces
QOUMF2B - 40 pieces
QOUMF3B - 24 pieces
Was this helpful?
What can we do to improve the information ?