Technical FAQs

Ask a Question

Can the SK5668 mounting kit be used to replace A1B breakers in an NA1B panel?

Issue:
Can the SK5668 mounting kit be used to replace A1B breakers in an NA1B panel?

Product Line:
Panels

Environment:
NA1B panels

Cause:
replacement breakers

Resolution:
No. These panels and breakers are obsolete, and there is no mounting kit available to retrofit currently available breakers into these panels.
Need to replace with QO/QOB type panel.


 
Was this helpful?
What can we do to improve the information ?