Technical FAQs

Ask a Question

Can you wire the 8660 Alphapak softstarter for Full Voltage Bypass?

Issue: Can you wire the 8660 Alphapak softstarter for Full Voltage Bypass?
 
Product Line: 8660 AlphaPak starters
 
Environment: All
 
Cause: N/A
 
Resolution:  No, the softstarter will trip with a fault because it was not designed to have a full voltage bypass. NOTE: The 8660 AlphaPak are obsolete. No parts, Service, or support are vailable.


CTA-ID : 7209
Was this helpful?
What can we do to improve the information ?