Technical FAQs

Ask a Question

Can you use a manual starter as the disconnect ahead of the contactor feeding the LH4N? This is 575 volt application for Canada.

This is not the same as an isolation contactor since it can not be operated automatically. It is not a problem with soft starter operation but there may be code and safety issues to consider. There must be overload protection.


CTA-ID : 7538
Was this helpful?
What can we do to improve the information ?