Technical FAQs

Ask a Question

Are the Alpha Pak 8660 starters available anymore?

Product LineClass 8660 AlphaPak starters


Environment: All 8660 AkphaPak starters

Cause:N/A


Resolution: No. The 8660 AlphaPak starters are obsolete. Replace with current ATS01, ATS22, or ATS48
Was this helpful?
What can we do to improve the information ?