Technical FAQs

Ask a Question

Can you put a Alpha Pak 8660 MGO46 unit for example on a smaller motor such as 20hp?

Issue: Can you put a Alpha Pak 8660 MGO46 unit for example on a smaller motor such as 20hp
 
Product Line: 8660 AlphaPak starters
 
Environment:All
 
Cause:N/A
 
Resolution:  As long as you use external overloads should not have a problem. Note. The Alphapak 8660 SSRVS are obsolete. No parts, service or support are available


 
Was this helpful?
What can we do to improve the information ?