Technical FAQs

Ask a Question

What is the power consumption and response time for the Masterpact NW and NT UVR?

Issue:  
What is the power consumption and response time for the Masterpact NW and NT undervoltage release?

Product Line:
Masterpact NW and NT

Resolution:
Power Consumption (VA or W)  Constant/Inrush  4.5/200 
Operating Threshold  Opening  0.35 to 0.70 Vn 
  Closing  0.85 Vn 
Circuit Breaker Response Time at Vn  NW  90 ms ±10 
NT  40 ms ±10 
Was this helpful?
What can we do to improve the information ?