Technical FAQs

Ask a Question

Why are shorting contactors unavailable for the smaller enclosed ATS46 softstarts?

The shorting contactors are only available above 30 HP on enclosed units.
On smaller Soft starters they are not needed because the current on the SCRs is lower.

CTA-ID : 7338
Was this helpful?
What can we do to improve the information ?