Technical FAQs

Ask a Question

Can an Altistart softstart be used on a wye delta, 2-Speed, or part winding motor?

Yes, wire the motor for the high speed (delta) or full winding configuration.
When sizing the unit, size it for the high speed winding current of the motor.
Make sure the full load amps of the motor is within the rating of the soft starter.


CTA-ID : 7376
Was this helpful?
What can we do to improve the information ?