Technical FAQs

Ask a Question

What is the replacement for IK and KI I-Limiter ILINE breaker like the IK36200 and KI36200?

Issue:
What is the replacement for IK and KI I-Limiter ILINE breaker like the IK36200 and KI36200?

Product Line:
Current Limiting 250A Frame PowerPact J with R Interrupt rating

Environment:
200KA requirement at 240Vac and 480Vac

Cause:
Need replacement for for the IK and KI breakers.

Resolution:
The replacement for the IK and KI breakers whether they are I-Line or unit mount are the PowerPact JR frame breakers.
JRA36150
JRA36175
JRA36200
JRA36225
JRA36250
JRL36150
JRL36175
JRL36200
JRL36225
JRL36250 
These are also available with electronic trip units.
 
Was this helpful?
What can we do to improve the information ?