Technical FAQs

Ask a Question

Wants to convert DC drive and motor to an Altivar ATV61/71 and AC motor.

Issue:
Wants to convert DC drive and motor to an Altivar ATV61/71 and AC motor.

Product Line:
Altivar ATV61 ATV71

Environment:
All .

Cause:
They want to remove an old DC motor and install a new AC motor and add an AC drive to work on the new AC motor.

Resolution:
Contact Regional Drives PAE Specialist to assist with this application.


CTA-ID : 7103
Was this helpful?
What can we do to improve the information ?