Technical FAQs

Ask a Question

Can the isolation contactor used with an ATS46 soft starter be NEMA type rather than IEC?

You can use either NEMA or IEC contactors.
The isolation contactor shall be sized for AC1 duty or greater.
The contactor must be able to close within 200 mS of the start command.


CTA-ID : 7477
Was this helpful?
What can we do to improve the information ?