Technical FAQs

Ask a Question

Do we use Resistive or inductive current when sizing an Altistart ATS46 shorting contactor?

You will use the Resistive current when sizing a shorting contactor.
This is AC1 rating. It is not necessary for the shorting contactor to be rated for the inrush current of the motor because the initial starting is performed by the soft starter.


CTA-ID : 7479
Was this helpful?
What can we do to improve the information ?