Technical FAQs

Ask a Question

What are the 24 volt replacement unlatch and latch coils for the 8903 SJ lighting contactor?

Unlatch - 31096-403-03 for 60 Hz.
Electrically Held Latch - 31104-400-50 for 60 Hz. and 50 Hz.
The mechanically held latch coil is not available in this voltage.

CTA-ID : 7605
Was this helpful?
What can we do to improve the information ?