Technical FAQs

Ask a Question

What are the LSIG trip unit functions on a new Micrologic trip unit?

Issue:
What are the LSIG trip unit functions on a new Micrologic trip unit?

Product line:
Micrologic and Powerpact electronic breakers

Environment:
Distribution equipment

Cause:
Need to know the definitions

Resolution:
LSI = Long-time + Short-time + Instantaneous Protection+ Ground fault
Available on the UL Listed, ANSI Certified, and IEC Rated 3.0 3.3,5.0, 5.0A, 5.0P, 5.0H, 5,3,6.0A,6.0P,6.0H, 6.3 trip units


CTA-ID : 7967
Was this helpful?
What can we do to improve the information ?