Technical FAQs

Ask a Question

Do the cooling fans for the Altistart ATS23 turn on based on temperature or do they run all the time?

Issue:   Do the cooling fans for the Altistart ATS23 turn on based on temperature or do they run all the time?
 
Product Line:   ATS23
 
Environment:  All
 
Cause:   N/A
 
Resolution:   The cooling fans for D72N - M12N will turn on at 50* celsius


 
Was this helpful?
What can we do to improve the information ?