Technical FAQs

Ask a Question

How does start/stop control wire on the 8660 SSRVS old style unit?

Issue: How does start/stop control wire on the 8660 SSRVS old style unit?
 
Product Line: 8660 AlphaPak starters
 
Environment: All
 
Cause:N/A
 
Resolution: A Stop pushbutton is wired between terminals 1 and 2, a Start pushbutton is wired between terminals 2 and 3. Must supply 115 volts ac on terminals 4 and 5. NOTE: the 8660 AlphaPak SSRVS are obsolete. No parts, service, or support are available


CTA-ID : 7262
Was this helpful?
What can we do to improve the information ?