Technical FAQs

Ask a Question

Does the 8660 old style starter have underload protection? Could a Motor Saver be used?

Issue:Does the 8660 old style starter have underload protection? Could a Motor Saver be used?
 
Product Line:8660 AlphaPak starters
 
Environment:All
 
Cause:N/A
 
Resolution: No, underload protection is not available. Could use a Motor Saver but only on the line side or else it would nuissance trip often.  NOTE: The 8660 AlphaPak SSRVS are obsolete. Parts, Service, and Support are no longer available

 
Was this helpful?
What can we do to improve the information ?