Technical FAQs

Ask a Question

What is the Electrical Interlock Kit for a HU661DS, Series E1 safety switch?

Issue:
Switch Accessories

 

Product Line:
Heavy Duty Safety Switches

 

Environment:
NEMA 4X

 

Cause:
Need for Electrical Interlocks


Resolution:

Two Electrical Interlocks are available for this 60A, 6-Pole, 600V Not Fusible Heavy Duty NEMA 4X Stainless Steel Switch:

EK10201 provides (1) Normally Open and (1) Normally Closed Sets of Contacts

EK10202 provides (2) Normally Open and (2) Normally Closed Sets of Contacts



CTA-ID : 6445
Was this helpful?
What can we do to improve the information ?