Technical FAQs

Ask a Question

What is the consumption of the control coil for 8502 SH contactor?

1780 VA inrush and 48 VA sealed for 60 hertz or 1960 VA inrush and 59 VA sealed for 50 hertz, this applies for all electrically held voltages. 1530 VA inrush for 60 hertz or 1250 VA inrush for 50 hertz, this applies for all mechanically held voltages. This also applies to all 8536 SH, 8538 SH, 8539 SH, 8606 SH, 8630 SH, 8640 SH, 8702 SH, 8736 SH, 8738 SH, 8739 SH, 8810 SH, and 8903 SH, 8940 S Size 6 excep ``NP`` devices.



CTA-ID : 4699
Was this helpful?
What can we do to improve the information ?