Technical FAQs

Ask a Question

What is the consumption of the control coil for 8502SA contactor?

For Series A - 245 VA inrush and 27 VA sealed for 60 hertz or 232 VA inrush and 26 VA sealed for 50 hertz. For Series B - 165 VA inrush and 33 VA sealed. This also applies to all 8536SA, 8538SA, 8539SA, 8606SA, 8630SA, 8640SA, 8702SA, 8736SA, 8738SA, 8739SA, and 8810SA devices. For enclosed devices, the series information is based on device and not enclosure nameplate.


CTA-ID : 4793
Was this helpful?
What can we do to improve the information ?