Technical FAQs

Ask a Question

What is the replacement 110-115 volt coil for a Type SG NEMA Size 5 contactor or starter?

The 110-115 VAC replacement coil for all Size 5 contactors and starters depends on the device`s series or revision. The following outlines the part by Series number: Series A 50hz - 31096-400-09, Series B - 50/60hz - 31096-320-50. For enclosed devices, the series information is based on device and not enclosure nameplate.


CTA-ID : 4799
Was this helpful?
What can we do to improve the information ?