Technical FAQs

Ask a Question

Can you put an output contactor between the motor and the output of the Altivar ATV66 drive to cycle motor off and on?

It is not recommended because when the contactor opens while running it can damage the IGBT`s ( output devices ).

This is not a suitable application for starting and stopping a motor that is running.


CTA-ID : 6967
Was this helpful?
What can we do to improve the information ?