Technical FAQs

Ask a Question

Where are the A1, B1, and C1 connections on the Altistart ATS23?

They are across the line, 1L1, 3L2, and 5L3 connections but on the U70, D12, D16N or D30N you do not have A1 (A2), B1 (B2) and C1 (C2) connections for the shorting contactors.

CTA-ID : 7280
Was this helpful?
What can we do to improve the information ?