Technical FAQs

Ask a Question

Is there a timing problem using Nema rated contactors as shorting or isolation contactors on the Altistart ATS23?

No - the Nema rated contactors have a pick up time of 75ms (worst case) and the ATS23 allows 200ms.


CTA-ID : 7304
Was this helpful?
What can we do to improve the information ?