Technical FAQs

Ask a Question

What are the specifications for the R2 relay on an Altistart ATS46?

The minimum switching capacity: 100mA - 24 Vdc
Maximum operating Voltage:400V

Rated operating current:
0.5A Inductive: 240Vac or 48Vdc
5A Resistive: 240Vac or 48Vdc
A relay may be required for larger shorting contactors.
This is a dry contact labeled R2A to R2C.
It is a Normally Open non-programmable contact.


CTA-ID : 7439
Was this helpful?
What can we do to improve the information ?