Technical FAQs

Ask a Question

What is the replacement power contact kit for an 8502 SA Contactor?

The replacement contact kit for all NEMA Size 00 (i.e., SA) contactors depends on the device`s series or revision. The following outlines the part by Series number: Series A - 3-Pole Kit 9998 SL2, 4-Pole Kit 9998 SL12. Series B - 3 Pole Kit 9998 SJ1.

This also applied to all 8536 SA, 8538 SA, 8539 SA, 8606 SA, 8630SA, 8640 SA, 8702 SA, 8736 SA, 8738 SA, 8739 SA, and 8810 SA, devices. For enclosed devices, the series information is based on device and not enclosure nameplate.

CTA-ID : 7618
Was this helpful?
What can we do to improve the information ?