Technical FAQs

Ask a Question

What are the trip curves for s 125 amp frame EDB, EGB, and EJB breaker?

Product Line:
Circuit Breakers

Environment:
Applies to ED, EG, EJ, EDB, EGB, EJB type breakers

Resolution:
The trip curves number listed below.

515-1     ED, EG, EJ,  15-20A, 1, 2, and 3 pole
515-2     ED, EG, EJ,  25-30A, 1, 2, and 3 pole
515-3     ED, EG, EJ,  35-50A, 1, 2, and 3 pole
515-4     ED, EG, EJ,  60-70A, 1, 2, and 3 pole
515-5     ED, EG, EJ,  80-100A, 2 and 3 pole
515-6     ED, EG, EJ,  110-125A, 2 and 3 pole

Link trip curve:

products.schneider-electric.us/technical-library/

CTA-ID : 9683
Was this helpful?
What can we do to improve the information ?