Technical FAQs

Ask a Question

What are the repair parts for a HU361RBEI Series E2 Heavy Duty Safety Switch?

Issue:
Repair Parts

Product Line:
HD SS

Cause:
Maintenance

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 40566-668-50 (arc suppressor NOT included)
Arc suppressor assembly - 40566-694-51
Lug assembly - 40251-016-52
Line base mounting screws - 21427-171-61
Handle knob kit - 4028344050K ( Series E Switches only)
Nema Type 3R cover hinge screw - 21427-171-61
Electrical interlock kit - EK3001 or EK3002


CTA-ID : 9233
Was this helpful?
What can we do to improve the information ?