Technical FAQs

Ask a Question

What are the repair parts for the H464DS, series F5? (may be shown as F05)

Product Line:
Heavy Duty Safety Switch, catalog number H464DS, Series F5

The repair parts for the H464DS, series F5 (F05) are as follows. These are the parts that can be replaced. No other parts are replaceable.
Complete Line Base - 4056703750 - (requires one line base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Line Base mounting screws - 40205-142-02 (requires 12 per line base)
Load Base Assembly - 40566-782-50 (requires one per phase - includes phynolic base, lugs and fuse clips)
Load Base mounting screws - 40205-142-02 (requires 2 per load base)
Arc Suppressor Assembly - 40566-775-50 (requires one per phase)
Arc Suppressor mounting screw - 40205-145-01
Lug Assembly - CL20F (incl. 6 lugs - requires mounting screws below)
Lug Assembly mounting screw - 21401-222-40 (per lug)
Switch Mechanism - 40567-401-50 (also requires mechanism coupling assembly 40566-998-50 and interlock connector assembly 40567-188-50)
Switch Mechanism mounting screws- 21949-181-21 (requires 2)
Handle Assembly - 40567-368-50
Lockplate - 40567-389-01
Lockplate mounting screws - 21949-181-21 (requires 2)
Was this helpful?
What can we do to improve the information ?