Technical FAQs

Ask a Question

What are the repair parts for the DTU223, series F5? (may be shown as F05)

Repair parts

Product Line:
Double Throw Safety Switch

Repair parts



The repair parts for the DTU223, series F5 (F05) are as follows. No other parts are available.
-Line Base - 4056683850 (one each upper and lower. Order arc suppressor, load lugs, and wire assembly separately).
-Line Base mounting screws - 4020515101 (requires 3 per line base).
-Arc Suppressor Assembly - 4056635550 (requires 1 per line base).
-Arc Suppressor mounting screw - 4020514501 (requires 1 per arc suppressor).
-Wire Assembly- 4056780050 (requires 1 per phase. Includes cable factory connected mechanical lug at one end and at other end a crimped connector. Use mounting screws of line and load lugs.)
-Line and Load Lug Assembly - 4025101851 (per lug - line, load)
-Line, Load Lug mounting screw - 4020514202
-Ground Lug - 4025101851 (per lug).
-Ground Lug mounting screw - 4020514801
-Switch Mechanism - 4056646950 (each for upper and lower).
-Linkage Assembly - 4056682750 (links together upper and lower switch mechanisms).
-Linkage Assembly mounting screws - 2299940562 (requires 7).
-Handle - 4056688750
-Lockplate - 4056673301
-Lockplate mounting screws - 2299940562 (requires 2)
-Cover Latch -40566-072-01 (each for upper and lower. Also requires cover latch spring)
-Cover Latch Spring - 4022304301 (each for upper and lower. Also requires cover latch)

CTA-ID : 9909
Was this helpful?
What can we do to improve the information ?