Technical FAQs

Ask a Question

Is replacement control coil available for 8910SYD368V08?

The 208 vac replacement coil for all 8910SYD368 8910SYD368 contactors depends on the device`s series or revision. The following outlines the part by Series number: Series A 60hz - 31096-400-15, Series B - 60hz - 31096-320-15. Series A coil consumption is 2970 VA inrush, 212 VA sealed for 60 hertz applications or 2970 VA inrush, 250 VA sealed for 50 hertz applications. Series B coil consumption is 1300 VA inrush and 14 VA sealed for 50/60 hertz applications.

CTA-ID : 10307
Was this helpful?
What can we do to improve the information ?