Technical FAQs

Ask a Question

What Class of fuse does the H228N, H228NR and H228NAWK safety switches accept?

Issue:
Class of Fuses

Product Line:
Heavy Duty Safety Switches

Environment:
Fuse Type

Cause:
Application

Resolution:

These switches accept Class L fuses ONLY. With Class L fuses installed, the switches are UL listed for use on systems with up to 200,000 RMS Symmetrical Amperes available fault current.


CTA-ID : 11100
Was this helpful?
What can we do to improve the information ?