Technical FAQs

Ask a Question

Is 21 volt replacement control coil available for LC1D4011?

21 volt control is not an option on theses contactors. Average coil consumption is 200 VA inrush 20 VA sealed for 50 hertz, 220 VA inrush 22 VA sealed for 60 hertz and 245 VA inrush 26 VA sealed for 50/60 hertz.

CTA-ID : 11137
Was this helpful?
What can we do to improve the information ?