Technical FAQs

Ask a Question

Is 21 volt replacement control coil available for LC1D15000?

21 volt control is not an option on theses contactors. Average coil consumption is 300 VA inrush 22 VA sealed for 50 hertz, 300 VA inrush 22 VA sealed for 60 hertz and 280 to 350 VA inrush 2 to 18 VA sealed for 50/60 hertz.


CTA-ID : 11142
Was this helpful?
What can we do to improve the information ?